Busbar Information
The most commonly used information about the busbar genie displays by default.
When the Advanced Properties box is selected, the table expands to include everything that is known about the selected busbar(s).
Basic busbar information includes:
Column |
Description |
---|---|
State |
Normal ( |
Page |
Name of the page on which the genie is found (displays only from the folder level). |
ID |
This is the busbar number, assigned when adding it to a page of a one-line. |
Busbar Errors
Before you use the drawing, correct all errors; otherwise the project might not compile and the animation will not work.
Errors that you might see for busbars are:
State |
Solution |
---|---|
Errors ( |
|
Busbar number must be a number greater than 0. |
The busbar number is missing, or it is less than or equal to 0. Add or change the busbar number. |